10/29/2020 6:38 PM | |
Posts: 1 Rating:
|
I´m having an issue with the ppp already installed. I have change the /etc/ppp/peers/provider and /etc/networking/interfaces files. When I execute the pon provider command, ppp0 network starts perfectly. But on boot, the ppp0 network starts fine, but when I try to ping google.com I have problems. If I execute poff provider and pon provider, everything start correctly again. Where do you think I should look for? Is there anything starting also on boot that affects the connection? Thank you in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2020 09:02:11New subject after splitting |
|
10/30/2020 9:59 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, pppd comes preinstalled in the example image, but our built-in network manager is actually using ofono for cellular connection. Since you have already configured pppd though, it might make sense to just run the pon command in a startup script at boot? You can check out this guide on how to create such a startup script. Best regards! |
Last edited by: Fe_lipe at: 10/30/2020 10:00:24 |
|
Follow us on