11/24/2020 12:36 AM | |
Posts: 1 Rating:
|
DEAR COMMUNITY I'm new in plc programming and when I download the tutorial of basic proramming of plc from SCE they used a iot2000 as CPU!!!! My questions: 1- Is the iot20xx can be used as a controler (programmed in ladder, FBC ...)? 2- If so where are its IOs? 3- How it can be used as a iot gateway in the industry physiquely (wirring)??? Thanks for answring ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2020 10:37:17New subject after splitting |
|
11/24/2020 8:05 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, the SCE is offering the so-called IOT2000EDU, which is a PLC for the IOT2040. This can only be used for educational purposes (in schools, universities, etc.).
The IOT2000EDU is more for learning programming in TIA Portal and not to be used as gateway. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on