4/27/2012 11:36 AM | |
Posts: 1064 Rating:
|
Suggestions would be for changes or inprovements to the forum Meet and talk general chat with other members like the weather ,sports score |
4/27/2012 11:53 AM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
For suggestions I am fully AGREE with you. If you have any suggestion or any feedback, you should post it in Suggestions - Feedback conference. If you will post in Meet & talk, Mods will transfer it For any other discussion - Like any techincal discussion which you cant find any suitable conference, or you have any general question regarding forum or any other thing then you can post them in Meet & Talk Also you can do general chat or congrats any person in Meet & Talk For Example, feefback and suggestion for campaign is in already in Suggestions - Feedbackwhile this thread is in Meet & Talk I hope it is clear now Regards Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
1 thankful Users |
4/27/2012 12:13 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Dear RAJKIRAN, I already replied that this thread is in Meet & Talkso it is correct Regards Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|