1/31/2013 7:55 AM | |
Joined: 1/29/2013 Last visit: 8/20/2023 Posts: 33 Rating:
|
Steady green led. No BF failure. Monitoring variable: No Byte uploaded but word-upload succeed. I can see there is a module problem or maintainens need. I will try to mirror to assembly. make the Master Slave and vv. AttachmentResults.zip (372 Downloads) |
1/31/2013 10:49 AM | |
Joined: 1/29/2013 Last visit: 8/20/2023 Posts: 33 Rating:
|
This is the result ofThe new projekt, reversing the Master to Slave and vv. i have copied your code and assignments. AttachmentReverseM.zip (348 Downloads) |
1/31/2013 1:30 PM | |
Joined: 1/29/2013 Last visit: 8/20/2023 Posts: 33 Rating:
|
I loaded "your" project inte the units. In IB21 there was nothing. |
1/31/2013 5:19 PM | |
Joined: 1/29/2013 Last visit: 8/20/2023 Posts: 33 Rating:
|
I.m happy It works. Major problem seems to be Profibus speed. It was set to 1,5Mb/s. It works if I reduce speed to 187,5Kb/s. My teacher hinted me. I'm still very greatful for your help and I realy cant tell if I'd been able to make this happen myself.And.... I learned o lot around this problem. I now know how to monitor variable status for example. I'm a beginner and I really don't know what code I can remove butit works. I can push a Button connected to to the slave, a bit is placed in a Byte, the system transfer the Byte to the Master where i is placed in an other bit which actuate a valve and the cylinder is advancing. Simple but beatiful. Now I will continue and solve the programming problem which was the origin task. Thank you very much. Mr Lof AttachmentReverseM.zip (369 Downloads) |
Follow us on