3/13/2024 3:00 PM | |
Joined: 6/20/2023 Last visit: 2/20/2025 Posts: 45 Rating:
|
p.s. Here's a box which confirms that I have S7 Professional installed. |
3/14/2024 5:53 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, there is (was) such a message indeed. And the remedy is to install the latest update. Unfortunately i can not remember which update it was and if it was for PLCSIM, STEP7 or ALM. Nevertheless, install all the latest updates for all packages. The message should be gone afterwards. There should also be another post to the same topic which was not too long ago. ***EDIT*** Cant simulate S7-1200 with basic licenseregards sancruz |
Last edited by: sancruz at: 03/14/2024 05:57:17Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
3/14/2024 8:50 AM | |
Joined: 6/20/2023 Last visit: 2/20/2025 Posts: 45 Rating:
|
@Hati, Hi, I start PLCSIM from the top pane of TIA Portal. |
3/14/2024 11:03 AM | |
Joined: 6/20/2023 Last visit: 2/20/2025 Posts: 45 Rating:
|
Hi, Reading your earlier post @sancruz, maybe I need the Service Pack 1 Update [?] See Picture. |
3/14/2024 11:54 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, please use the latest version for both, PLCSIM and STEP7, this was also the solution in the other topic. Updates for STEP 7 V18, S7-PLCSIM V18 and WinCC V18-> STEP 7 / WinCC V18 Update 3 -> S7-PLCSIM V18 SP2 (08/2023) regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
3/14/2024 2:47 PM | |
Joined: 6/20/2023 Last visit: 2/20/2025 Posts: 45 Rating:
|
HI SanCruz, I installed SP1 and SP2. PLCSIM is now working again! Many thanks! |
Last edited by: Masood01 at: 03/14/2024 14:47:35 |
|
This contribution was helpful to
2 thankful Users |
Follow us on