(0)| 11/13/2012 9:27 PM | |
|
Posts: 4 Rating:
|
Hi Experts, I'm trying to find any information about make a system Redundancy With S7400-H and Profinet, so I found in the user manual: "profinet_system_description_en-US_en-US.pdf" that we can do it using a CPU 414-5 H PN/DP and IM153-4 PN HF V4.0 (ET200M). Attachment400H_Redundancy_ET200SP-M.zip (1680 Downloads) |
Last edited by: Dony C. at: 11/15/2012 1:07 AMOK, Now I have done a HW Configuration using "IM 155-6 PN ST (ET200SP - 6ES7 155-6AA00-0BN00)" and "IM153-4 PN HF V4.0. (ET200M)" in redundancy with a CPU 414-5 H PN/DP, so I have compiled in HW Configuration and also in NetPro with no errors. Can anybody tell me if this configuration is going to work correctly when I download it into S7400H PLC?? Please take a look to the "PROFINET IO Topology" in HWConfig. I attach the Archived Project, so I hope somebody can help me, and if the HW Config. is good also hope I can help to somebody. Thanks for your Help.!! Last edited by: Dony C. at: 11/13/2012 9:30 PM |
|
Follow us on