5/19/2007 2:51 AM | |
Posts: 5 Rating:
|
Thanks for your help. The system is going to be assembled next week, so i´ll let you know. |
5/19/2007 1:31 PM | ||||
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Jelbo, You need a communication which have PDM-Routing capabilitys and then it will work. The Routing capabilitys for PDM are not the same as for the normal routing capabilitys for the CPs and the CPUs!!
For routing thrue the CP443-5DX04 please see the FAQ Configuration of field devices with SIMATIC PDM via Industrial Ethernet / DS routing When you use a Routing of S7 and of Data Sets (PROFIBUS DP) via the Link Gateway IE/PB then it will only work when you are using PDM integrated into STEP7 and having the right licenses. |
|||
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
||||
This contribution was helpful to
1 thankful Users |
Follow us on