9/13/2017 5:39 AM | |
Posts: 49 Rating:
|
Hi all, I add the one AO card in the hardware configuration for my S7-412-5H. after that i went to download that time it shows 13:5799 error(profinet differ from the online and offline). i searched error code. this code only not available. before modified i went to online,it was fine. after modified this one showing. i uploaded the backup, compare SDB and went online all are fine. after modified for AO card, i cannot to download with this backup also. it shows same issue. We are using following configuration S7412-5H with CP and 3rack of IM154-HF with media redunancy protocol can you please anyone advice about this issue. Attachmenterror.zip (372 Downloads) |
Last edited by: PlUg & PlAy at: 9/13/2017 8:17:21 AM |
|
9/19/2017 3:14 PM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Hello PlUg & PlAy, Sorry for the delay. I don't think you have a chance to do this online. It's restricted with Profinet IOs to be changed/modified online.
Best regards, H-H |
This contribution was helpful to
1 thankful Users |
9/24/2017 6:58 AM | |
Posts: 49 Rating:
|
Hi H-H,
Thanks for your reply. while hardware configuration downloading can i select the download in stop mode. If i select this option, it will accept the modified configuration. Thanks, Plug & play |
10/16/2017 10:53 AM | |
Posts: 49 Rating:
|
Thanks, After download in stop mode . working fine |
This contribution was helpful to
1 thankful Users |
Follow us on