8/20/2018 9:02 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello Caleb; Generally, writing to a S7-400 memory card (Flash EPPROM) is generally done when inserted in the CPU. That is the easoiiest way. There is an alternative: you can use the integrated card reader of a Siemens PG (I believe the external model is no longer available from Siemens) to read or write to S7-400 memory cards. This is discussed in the following manual: SIMATIC Programming device SIMATIC Field PG M5 https://support.industry.siemens.com/cs/ww/en/view/109482603 Notice: do not attempt to use a non-Siemens card reader for this operation. Siemens memory cards are formatted uniquely for Siemens operations, and a standard card reader will start by formatting the memory card to Windows structures, which will make the memory card unusable for a Siemens CPU. Hope this helps, Daniel Chartier |
Follow us on