11/13/2018 8:41 PM | |
Joined: 12/10/2015 Last visit: 7/13/2025 Posts: 6 Rating:
|
Dear experts, I looking forward for your help. I have S7-400 H System consists of two 412-5 H PN/DP [6ES7 412-5HK06-0AB0 / V6.0] and 10 ET 200M IM 153-2 [6ES7 153-2BA02-0XB0] in order to connect more than 1700 IO Signals. I used to increase the number of IOs so I brought two ET 200M IM 153-2 [6ES7 153-2BA10-0XB0] since the previous model is already obsolete. I have a backplane bus modules [6ES7 195-7HB00-0XA0] to insert the new cards. I made the hardware configuration and I downloaded it to the CPU but unfortunately it’s giving me the (Module not available), or as attached below. Please help. Thanks in advance. AttachmentFauly Modules.pdf (474 Downloads) |
11/14/2018 9:56 AM | |
Posts: 101 Rating:
|
Hi , you can found more infos here : https://support.industry.siemens.com/cs/attachments/46387818/et200m_interface_modules_product_information_fr-FR_fr-FR.pdf?download=true Attachmentet200m_interface_modules_product_information_fr-FR_fr-FR.pdf (530 Downloads) |
Last edited by: IssamWTL at: 11/14/2018 9:57:26 AMLast edited by: Jen_Moderator at: 11/14/2018 11:32:05 AMAdded PDF file as an attachment. |
|
This contribution was helpful to
1 thankful Users |
10/21/2019 4:03 PM | |
Joined: 3/28/2019 Last visit: 11/6/2023 Posts: 17 Rating:
|
How can I change my ET 200M's buffer battery on run mode? Thanks |
Follow us on