3/18/2025 8:11 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi Savisar, In this case, in order to check what could be going on I would recommend you to first check the following: - Perform the error logic (STEP 7) and share with us the initial message received from the block: "How do you evaluate the status of system blocks in STEP 7 (TIA Portal)?" - Screenshot of the block online to see the behavior and inputs. - Additionally, when using the CP you have to have a license to be able to work as you can see in the following link: "How do you configure a Modbus/TCP communication for a SIMATIC S7-300/S7-400 and where can you find further information?" Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on