9/18/2025 8:03 PM | |
Joined: 7/19/2023 Last visit: 9/19/2025 Posts: 1 Rating:
|
Hello, I'd like to download data to S7-1200 from the following address: https://api.raporty.pse.pl/api/rce-pln In order to establish https connection I downloaded to the PLC certificates from the website as described in section 2.3 of the manual: I tried using LHTTP_Get function from LHTTP library, but it returns error with status code 8601 and subfunction status code 80E4 what means No valid certification authority found from TCON function. When I try to download similar json from the http server working in the local network (without TLS) everythink works ok. PLC 1211C with firmware 4.6. Tia Portal V19. |
9/18/2025 8:29 PM | |
Joined: 7/7/2010 Last visit: 9/23/2025 Posts: 16136 Rating:
|
The LHTTP library is for S7-1500 PLCs. To do what you want means you need to replace the s7-1200 with an s7-1500 PLC.
|
science guy |
|
Follow us on