11/17/2006 3:30 PM | |
Posts: 21 Rating:
|
Why cant i do copy RAM to ROM function on CPU 318-2 CPU. If i have to save the program on flash memery, how should i do it? rgds |
11/21/2006 12:14 PM | |
Joined: 9/1/2006 Last visit: 8/21/2025 Posts: 193 Rating:
|
Hi guys, I think Pegaia has it wrong this time... With the new MMC CPU's you need to use "Copy Ram To Rom", the other function is used for older CPU's or S7-400 CPU's that use the big memory cards. See MMC article http://support.automation.siemens.com/WW/view/en/22295462 regards, René |
Follow us on