(0)| 9/1/2005 3:43 PM | |
|
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating:
|
It seems you PCMCIA card simulates a serial port (COM) not very well and therefore can´t be used for LOGO!. As your PC has no serial port, the only alternativ solution is to use a USB/serial converter. In Internet are two USB/serial converters described, which work with LOGO!. Many other USB/serial converters can be used with LOGO!, but not all. http://support.automation.siemens.com/WW/view/en/11611048 |
Last edited by: O_Moderator at: 12/14/2010 1:44 PMlink edited |
|
Follow us on