(0)| 6/16/2021 2:07 PM | |
|
Joined: 11/28/2015 Last visit: 7/18/2025 Posts: 4 Rating:
|
I'm having the same question: simulate a HMI, but using an Access Address NAT IP address to connect. PLC no issue, as I can use Extended go online with the NAT IP of the PLC filled into the Access Address, but I cannot find a similar function for simulating an HMI. Preferably, I do not want to change any properties in my project. So only setting a 'temporary' access address would be great. PG/PC interface etc seems fine, though I am not familiar with having to setup things here. I only select the correct adapter, that's it.. Can I somehow set the NAT IP address, or routing to the PLC, there? ------------------------------------------------------------------------------------------ |
Last edited by: Han1988 at: 06/16/2021 14:07:55Last edited by: Han1988 at: 06/16/2021 14:08:17Last edited by: CS Moderator at: 06/16/2021 15:54:31New subject after splitting |
|
Follow us on