1/20/2019 4:22 PM | |
Joined: 12/18/2014 Last visit: 9/11/2025 Posts: 35949 Rating:
|
SINAMICS Blocks DriveLib for the control in the TIA Portal Here you can find the DriveLib for the control of SINAMICS S/G converter systems with SIMATIC S7-300/400/1200/1500 in the TIA Portal. The objective of the standard "Communication blocks for SIMATIC S7-300/400/1200/1500" blocks is the simple implementation of a cyclic or acyclic communication connection between a SIMATIC S7-300/400/1200/1500 controller and an axis of a SINAMICS S/G converter system. |
Last edited by: ixo65 at: 1/20/2019 5:47:40 PM |
|
This contribution was helpful to
2 thankful Users |
1/21/2019 7:41 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, just an additional information to your statement: SINAMICS V drives with Profinet communication (like V90PN) can also be used together with those blocks. And there are also additional libraries available now, which could be helpful: 1. https://support.industry.siemens.com/cs/ww/en/view/109747655 Here you find additional blocks for cyclical communication to SINAMICS drives. 2. https://support.industry.siemens.com/cs/ww/en/view/109760317 Here you find additional blocks for acyclical communication to SINAMICS drives (like an EncoderAdjustment FB). From time to time there could be added more blocks to those pages. |
With best regards, |
|
2/14/2022 11:49 AM | |
Joined: 4/21/2021 Last visit: 3/21/2023 Posts: 45 Rating:
|
Thankyou |
Follow us on