3/15/2022 6:36 AM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
Which versions of the example image did you try? If you are unlucky, you got a device with older firmware than the latest image supports. Then you need to follow https://support.industry.siemens.com/tf/ww/en/posts/firmware-upate-to-use-example-image-v1-2-1/275777/?page=0&pageSize=10 first. If that does not help, please attach a UART-USB cable (like used for Raspis as well) to X17 and report what the device prints during power-up. |
Follow us on