5/4/2022 1:13 PM | |
Posts: 5 Rating:
|
Dear Bergmanu, I have problem with changing boot order on a FS:04 iOT2050. Short description: Changing boot order under running example image 1.2.1 or 1.2.2 is not working. Meanwhile changing the boot order via serial connection (u-boot shell, via UART cable) is working well. Detailed problem: Trying to change boot order under running Example Image V1.2.2:
Than I interrupted the boot and checked the env variables from u-boot shell:
Then modified it under u-boot
Booted again into Example Image v1.2.2 and tried to modify it again:
I have tried it under running Example image v1.2.1 as well. Same symptom. The FS:04 came without pre-installed OS. This is clear, I've seen your post about it. Firmware version: 2021.04-V01.02.01-0-g40d3fc0 I tried to upgrade the firmware to 2021.04-V01.02.01.03-0-g7e29ca7
But it says not possible. May I ask you for all the released firmware to dowload? Same with released OSes. It is really not efficient to dif the forum for all the news about the releases and begging for dowloads. We are develeping a serious application running on this device but the poor documentation and continuous bugs slowly forces us to choose an other brand. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/04/2022 14:00:43New subject after splitting |
|
5/4/2022 2:28 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, thanks for your detailled description! With the new firmware the arguments of the boot_targets need to be put in quotation marks:
This has changed with the u-boot version being used in the firmware. Changed this in the documentation of the setting up. I understand your inquiry, but we can't upload each and every "old" OS and firmware. The latest OS for the new and old firmware is available. The firmware is not needed to be upgraded/downgraded on the FS:04 device. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on