5/13/2022 2:22 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, I would also have expected the same behavior as you, when activating the checkbox. In my case I don't even get a message when restarting the flow. I don't see any solution with the nodes functionality at the moment - neither to read at startup nor to read cyclically. Another realized that in another way: Writing the value periodically to a file from Linux and reading in the file from node-red. See here. You add a requirement for those two functionalities on github. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
1 thankful Users |
Follow us on