5/20/2022 2:03 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, I tried to install it on the latest Example Image V1.2.2 (Debian 11), but was not able to. The step 1 in the linked instructions needs to be changed for Debian 11. There is one existing for Debian 11 and it also contains the prod.list file: https://packages.microsoft.com/config/debian/11/. When I add this repository and follow the other steps, the package defender-iot-micro-agent is not available. I found some packages here, downlaoded it and transfered it to the IOT2050, but it seems that this is only for armhf not arm64... Did not find a way to install this software, sorry. Maybe Microsoft should update their docu for current Debian versions. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on