8/18/2022 3:21 PM | |
Joined: 3/23/2016 Last visit: 7/22/2025 Posts: 5 Rating:
|
Hi, i have the same problem: FB37 time stamp conflicts. If I try to open FB37 i receive a message "time stamp of the FB or SFB for symbol FB_P_SND_RK in FB37 is more recent the the time stamp of the logic block interface". So I think the problem are the versions of FB7 and FB8. I also tried to use the old version that i found in cp PtP>cp341-> called FB107 and FB108 and renamed as FB7 and FB8 but it does't work. does anyone have a solution? Thank you very much ------------------------------------------------------------------------------------------ |
Last edited by: zepego at: 08/18/2022 15:35:18Last edited by: Jen_Moderator at: 08/19/2022 10:23:44New subject after splitting |
|
8/22/2022 2:04 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello zepego, regarding to the message time stamp conflict we recommend to use the FAQ: How do you update invalid block calls (time stamp conflicts) in calling blocks? With best regards |
8/22/2022 2:13 PM | |
Joined: 3/23/2016 Last visit: 7/22/2025 Posts: 5 Rating:
|
Thanks Cicero. I don't know why my post was moved here to a new thread, because that way I'm afraid my problem is not clear. I have the problem with a protect FB of this post (link), but it is impossible to solve (i think) without the help of whoever made the block |
8/23/2022 7:02 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Hi zepego, you have posted your question in an old topic that contains a lot of posts and deals with communication function blocks. The issue your question is based on is not the main aspect of the original topic and has never been answered (Your quoted question from the original topic was posted in 2016). Therefore I have split your question to increase the probability that you will be helped. Best regards, |
This contribution was helpful to
1 thankful Users |
Follow us on