(1)| 10/16/2020 11:42 AM | |
|
Joined: 10/11/2006 Last visit: 12/22/2025 Posts: 6062 Rating:
|
Hello, the main advantage of a resolver is the robustness. Due to its construction based on inductive scanning (its a rotary transformer), it is more robust in areas with high vibrations or dust, compared to other encoder systems based on photoelectrical scanning, where a glass disc is inside. The disc can be easier damaged and is more sensitive for dust. But of course only very few application areas require such an additional robustness. Attached you find an extract from an old catalogue showing the construction principles. A disadvantage is the lower resolution compared to e.g. optical sin/cos encoders. Attachmentencoder systems from da_65_3_en_2004.pdf (1809 Downloads) |
|
With best regards, |
|
This contribution was helpful to
|
|
| 10/4/2022 12:20 PM | |
|
Posts: 8171 Rating:
|
New question published by baigshehroz is split to a separate thread with the subject resolver is not working. Best regards |
This contribution was helpful to
|
|
Follow us on