(1)| 9/29/2022 9:30 PM | |
|
Joined: 2/16/2022 Last visit: 7/24/2025 Posts: 4 Rating:
|
Hello everyone, I am trying to connect my PG 615 to a S5 100U. Unfortunately I don't have the original cable 3NET 810 1130-01, and used another 15/15 cable instead, which loops the pins 1:1. But this cable is missing pins 3 and 11. When I turn on the S5-100U, the PG 615 starts and shows the presets. But there the message number *6 is displayed, which according to the manual indicates a cable break. I also can not go ON-Line. There comes then the same message number *6. In the manual for the PG 615 you can see in picture 2.15 that pins 3 and 11 are not used. However, I suspect that the picture in the manual does not show all the pins used. Can anyone tell me if the original cable uses all 15 wires? Many thanks for your support, Manfred
|
| 9/30/2022 1:28 AM | |
|
Joined: 12/18/2014 Last visit: 1/11/2026 Posts: 36435 Rating:
|
Maybe this can help you.
Attachmente_6xxagu.pdf (1148 Downloads) |
Follow us on