(0)| 10/30/2022 7:20 AM | |
|
Posts: 7 Rating:
|
Hello my name is Karatsiolis Michael and I had problem with the electricity of my factory and the problem is all card of simodrive 611 was damage.I have replace all the cards and at the following video all the motors doesn't work when the machine is trying to work.We have Chek all the fuse and switches,the cambles the thermo switches and they work perfect!How can we resolve that problem because the machine doesn't work 3 months....Can you help me please!I have big problem with my work... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/02/2022 05:29:46New subject after splitting |
|
| 10/30/2022 9:05 AM | |
|
Posts: 8092 Rating:
|
Hello, Welcome to forum. You should have open this topic in SIMODRIVE Converter system product conference since it is related with 611 drive that too analog. In attached snap, it looks like ER module is enabled, spindle drive digital displays 5, probably pulse cancellation, but could not confirm since display parameter number is not known, Other axes modules display "n" which indicates parameter board detected & drive 663 & 65 terminals are enabled. With this inadequate information, could not help you much more, but suggests you below points to check. 1. Which is controller? 2. What alarm or fault is displayed on OP or HMI? 3. Check if DC voltage is available at 611A drive bus & how much it is? 4. What do you mean by card damage? Is it LT power module (to which motor connections are connected?) or control card (to which enable terminals & encoder connections are connected?) 5. Have you checked connected motors, cables etc. for ground or inter phase short circuit? 6. Have you replaced ER module? If yes, have you set DIP switch (provided at top of ER module) setting on ER module as per input supply voltage specification? Please refer SIMODRIVE 611 analog, Transistor PWM Inverters for AC Feed Drives and AC Main Spindle Drives manual for more detail information. Hope this helps. |
| 10/30/2022 9:31 AM | |
|
Posts: 7 Rating:
|
|
| 10/30/2022 9:31 AM | |
|
Posts: 7 Rating:
|
|
| 10/30/2022 9:32 AM | |
|
Posts: 7 Rating:
|
|
| 10/30/2022 9:32 AM | |
|
Posts: 7 Rating:
|
Fault F05 |
| 11/2/2022 10:04 PM | |
|
Joined: 10/17/2007 Last visit: 12/23/2025 Posts: 4566 Rating:
|
Are you sure you replaced correct control card? do you have the old control card? please post the parts number for the card SPECILA FOR SPINDLE Motor control--such as 6SN1112-????? From you last picture--I see at least one feed/axis drive is ready to run
|
|
If you like my comments please |
|
Follow us on