11/2/2022 9:40 AM | |
Joined: 6/23/2022 Last visit: 5/12/2023 Posts: 3 Rating:
|
Hi! I am wondering if there is something fundamental about the IOT2050 that makes it impossible to install a clean Debinan netinst image, or if I have done something wrong when following the setup guides. I am used to the SIMATIC IPC127E units, which we can boot from USB and install Debian on without any hurdles. I have tried to do the same for the IOT2050, but I never get to boot from the image. I am doing the following: => run bootcmd_usb0 |
11/2/2022 9:57 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, for a 127E this is the way to go and it works. For the IOT2050 you can't use the standard Debian OS. That's why we created a so-called Example Image, which is based on Debian 11. You can download it here and will find the sources to customize the image here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on