11/16/2022 12:51 PM | |
Joined: 1/21/2013 Last visit: 9/15/2025 Posts: 4109 Rating:
|
Hi Lakshay, you have a CPU 1212C, DC/DC/DC and asking for extending your setup using a ET 200SP, AI 2xU. These are two different product families! The AI module you are asking for can only be used in a ET 200SP setup. Such an setup can be accessed by the S7-1200 but you will need at least an ET 200SP Interface Module. A helpful tool to get information about possible hardware configurations is the TIA Selection Tool. You can use it for free! Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on