(1)| 10/26/2022 11:04 AM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, we have been working with 10 qty CPU 1518TF-4 PN/DP, on one PLC, we get the following: (see extract from PLC diag buffer attached) Event ID: 16# 02:4175 CPU error: Memory card evaluation error: Inconsistent external load memory structure current card type: Program card (external load memory) Function finished/aborted, new startup inhibit set: .. - External load memory is corrupt We have swapped SD cards between a working CPU and the suspect CPU and after also swapping card contents, the fault stays with the CPU, suggesting an error with the actual SD card hardware. My question is can there be anything HWConfig/software-wise that may cause this symptom or are we simply looking at a warranty type issue? Regards, Graeme AttachmentPLC_DIAGNOSTIC_BUFFER.txt (751 Downloads) |
| 10/26/2022 11:17 AM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
warranty, this is normal a defect in the SD Slot |
This contribution was helpful to
|
|
| 11/17/2022 6:16 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi Davide, thanks for the input. It's one of the first things we did after it happened a few times. We were hopeful that the firmware upgrade would solve it when we saw that the failures seemed to occur on older firmware initially. All our CPUs have now been upgraded to the latest firmware as attached. It has however, occurred on CPUs with the latest firmware regardless (as well as on CPUs with the latest hardware build revision) Regards, Graeme AttachmentMemory_Card.pdf (763 Downloads) |
Follow us on