(0)| 11/23/2022 2:25 PM | |
|
Posts: 1 Rating:
|
Hello everyone Can anyone give me the proof that it is possible to use S7 1500 software controller on a non-Simatic IPC? And if it is compatible, is it then compatible for every brand if I follow the features listed in one of the messages above? I heard somewhere that one of the last versions (21.9) of the CPU 1507 S can work on a non-Simatic IPC. But after following the manual "S7-1500 Software Controller CPU 1505SP (F/T/TF), CPU 1507S (F), CPU 1508S (F) Version 21.9" it did not work on my non Simatic IPC. I got a screen with the following error "Fatal error occured on core 0: Unsupported PC type 'HX500". So now without proof I am doubting that it is even possible to connect the Siemens software controller with a non-Simatic IPC. Thanks in advance. Kind regards. Jelle ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2022 08:35:58New subject after splitting |
|
| 11/23/2022 2:31 PM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
IT IS NOT POSSIBLE! |
Follow us on