(1)| 8/13/2020 9:20 PM | |
|
Joined: 3/17/2017 Last visit: 9/10/2025 Posts: 41 Rating:
|
Dear Experts, I would like to know if it's possible to use a mid-range S7-1500 series CPU with CM or CP module as PROFIBUS DP Master together with a number of older ET200B series remote I/O stations? CPU 1515-2 PN (6ES7 515-2AM01-0AB0) and Terminal Block: 6ES7 193-0CB10-0XA0 Software: TIA Portal/STEP7 Professional V15 Yes, I know that the ET200B devices have been discontinued back in 2015. But there are GSD files available (ca. year 2000). So, it looks like there is a possibility to link all of these devices together. Also, please recommend which module CM 1542-5 or CP 1542-5 is more suitable for this task. Thanks a lot in advance and Best Regards, s4gia |
Last edited by: s4gia at: 08/13/2020 21:26:31minor re-wording |
|
| 12/5/2022 9:00 AM | |
|
Posts: 8171 Rating:
|
New question published by tomo314 is split to a separate thread with the subject How to get x.200 gsd file?. Best regards |
Follow us on