12/14/2022 12:14 PM | |
Joined: 2/19/2020 Last visit: 1/26/2025 Posts: 57 Rating:
|
Dear all, I hope everything is ok with you. I have downloaded the GSD file for SIRIUS 3RW52 soft starter from the following link: https://support.industry.siemens.com/cs/de/en/view/109757789 After the installation of the GSD file, I tried to drag and drop the correspondent file (3RW% 2**-**C** V2.0) to integrate the new device into the DP network. In this context, the system warns me that “Module cannot be inserted here. You can use only DP slaves in a master system”. Could you please help me? Attach there is an image of the HW Config. Thank you. |
Last edited by: Jen_Moderator at: 12/15/2022 07:59:57Link optimized. |
|
12/19/2022 4:03 PM | |
Joined: 2/19/2020 Last visit: 1/26/2025 Posts: 57 Rating:
|
Hello Mr. Duris_I, Thank you for you answer! It helped a lot! |
This contribution was helpful to
1 thankful Users |
Follow us on