1/3/2023 8:53 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, we as Siemens do not offer a 24V Arduino shield with 8x DI and 8x DQ. We only have a 10x DI shield and the I/O Module with 5x DI and 2x DQ.. The only shield I found on google is this one: https://www.rugged-circuits.com/24v-industrial/24v-industrial-shield. But not sure whether this is available. I suppose you are talking about 24V IOs? Having a suitable 24V I/O shield is most challenging criteria in your application I guess. Basically reading / writing IOs is possible with each of the languages you mention. For python / C++ we use the mraa lib, for node-red we have suitable, pre-installed nodes for this. When it comes to support this forum is the only platform available, I will be there to support you the best I can. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on