(0)| 1/30/2023 3:01 PM | |
|
Joined: 1/9/2019 Last visit: 3/3/2025 Posts: 1 Rating:
|
In the past (2012), in https://support.industry.siemens.com/cs/document/60179485/delivery-release-for-motion-connect-drive-cliq-cables-with-m12-connector-for-direct-measuring-systems?dti=0&lc=en-ESit was stated that: "The maximally permissible overall cable length between measuring system and RJ45 socket at the SINAMICS S120 is 30 m." In the 2021 edition of the NC62 catalog: https://support.industry.siemens.com/cs/attachments/109746845/motion-control-NC62-complete-english-2021.pdf?download=truein page 8/41 there is a connection scheme with 3 possible connections for "Non-Siemens direct measuring systems with DRIVE-CLiQ interface with M12 connection". These connections allow for an overall cable length between DRIVE-CLiQ encoder and Control Unit of up to 100 meters. Please see picture in the attachment. Is this correct? Can I connect a third-party DRIVE-CLiQ encoder according to any of these 3 schemes in the latest NC62 catalog and the overall cable length is not limited to 30 meters any more? Is it possible to use DRIVE-CLiQ hub to have even greater overal cable length between DRIVE-CLiQ encoder and CU? |
| 1/31/2023 10:11 AM | |
|
Joined: 10/11/2006 Last visit: 1/8/2026 Posts: 6065 Rating:
|
Hello pdlfuente, |
|
With best regards, |
|
Follow us on