3/9/2023 8:39 PM | |
Joined: 12/28/2022 Last visit: 1/8/2025 Posts: 5 Rating:
|
Hi, All Question # 1 What is meaning and purpose of Hot swapable? [snip] Waiting for your kind response. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Ahtisham54 at: 03/09/2023 20:41:02Last edited by: Jen_Moderator at: 03/10/2023 08:46:13New subject after splitting Last edited by: Jen_Moderator at: 03/10/2023 08:46:38Division of questions into separate topics. |
|
3/10/2023 8:45 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by Ahtisham54 is split to a separate thread with the subject What is the maximum number of remote racks the S7-300 PLC can have?. Best regards |
3/10/2023 10:56 AM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello Ahtisham; The idea behind a "hot swap" is the possibility for an I/O module to be removed and replaced while it is still powered-up and connected to the CPU. The CPU should remain active during this operation without declaring a fault. PLCs that offer such a functionnality generally use a bsckplane to connect the CPU and the I/O mobules. A S7-300 CPU (since the other questions you ask refer to this family of CPUs) does not have a backplane structure , the I/O modules are connected using a U-connector. The S7-300 cannot use hot-swap functionality. In some special configurations a S7-300 can use so-called "active bus connectors" to use as a backplane, for redundancy topologies for example. But even then the S7-300 does not support hot-swapping, it does not have the required OB83 in its firmware. See the following discussion, Ayman Elotaify's answer is correct and very detailed. https://support.industry.siemens.com/forum/ca/en/posts/hot-swap/67961 Hope this helps, Daniel Chartier |
3/10/2023 11:30 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello Ahtisham; S7 PLCs refer to "hot-swap" of modules as CiR (Configuration in Run). Here is one example provided by SIOS for CiR on a Profinet system: https://support.industry.siemens.com/cs/ca/en/view/109770841 To locate more articles on applications for CiR, simply use the search box at the right of this page, use the search term "CiR". Once the SIOS page opens use the Knowledge Base filter to find documents such as you can see in the attached screenshot. The Forum filter will show requests for help from users wanting to implement CiR on different CPUs, and answers provided by members of the forum. Hope this helps Daniel Chartier |
Follow us on