4/5/2023 6:33 AM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Hello! Replacing an MM440 with V20, having som problems after this. My gear:400V 3KW FILT C3 6SL3210-5BE23-0CV0 and brake module 6SL3201-2AD20-8VA0 The lift only runs on 1Hz, though I have three fixed speeds. While jogging the motor runs, but very porly(choppy) While jogging the motor down, the motor goes up a bit, then standstills and triggers F6. Jogging UP the motor runs fairly fine, while a little choppy. Worked fine with the old MM440. Any parameters in the V20 that could be the problem? Tried altering boost with no luck Attatching the old parameter list from the MM440, these parameters where the only changes needed to run from factory defaults. Regards// |
Follow us on