(0)| 4/23/2023 5:26 AM | |
|
Joined: 4/15/2023 Last visit: 1/4/2026 Posts: 27 Rating:
|
1) Is the 6ED1052-1HB08-0BA0 a 0BA0 series Logo!? Or does it belong to the 0BA8 series? (this post says that the 6ED1052-1MD08-0BA1 Logo! is "a 0BA8 LOGO! of the 4th Generation")) 2) What type of hardware should be selected in Logo Soft Comfort 8.3 for network project with 6ED1052-1HB08-0BA0 (s7-1200 <-> Logo! ):
? |
Last edited by: pynista at: 04/23/2023 05:28:39Last edited by: pynista at: 04/23/2023 05:29:02 |
|
| 4/23/2023 5:37 AM | |
|
Joined: 12/18/2014 Last visit: 1/8/2026 Posts: 36419 Rating:
|
The LOGO! with the arcticle number 6ED1052-1HB08-0BA0 ist a LOGO! 0BA8 of the third generation, also called LOGO! 8.2 In the hardware selection you have to select "Logo! 8.1 & 8.2 (Logo! 8.FS4)".
AttachmentVersions of 0BA8.txt (834 Downloads) |
Last edited by: ixo65 at: 04/23/2023 05:48:11 |
|
This contribution was helpful to
|
|
| 4/23/2023 5:48 AM | |
|
Joined: 4/15/2023 Last visit: 1/4/2026 Posts: 27 Rating:
|
Thank you very much |
This contribution was helpful to
|
|
Follow us on