(0)| 4/29/2023 9:20 AM | |
|
Posts: 3 Rating:
|
Hello. I struggle with start operating PTO drive with PLC1512C. All parameters set like in manuals, both cases speed_axis and positioning_axis the same error in commisioning panel (fault in the drive) without possibility to erase it. I use many PTO drives at S7-1200 without any problems (often with strict positioning mode) and here on 1500 i cannot startup it at all. I downloaded sample project at 1511C (i see that i use exactly the same config) convert it to my 1512C and the same problem - fault in the drive. Ready input is disabled and no error input from the drive so how this info may appear? I checked telegram 3 and see that there is an error but how PLC generates it without such signals from servo? I have ordinary servo with only pulse and direction PTO signals - no encoders, ready inputs etc just pulses (position check at the external sensors just moving between) Cannot find any help on the internet and my ideas are exhausted - i use TIA15.1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2023 09:31:24New subject after splitting |
|
| 5/8/2023 9:05 AM | |
|
Posts: 3 Rating:
|
Done everything based on siemens manuals - pictures of configuration in attachments
AttachmentPTO.zip (479 Downloads) |
Follow us on