6/12/2023 9:42 PM | |
Joined: 4/6/2021 Last visit: 8/26/2025 Posts: 6 Rating:
|
Hi, I have two IOT2050 Advanced (6ES7 647-0BA00-1YA2), FS:02. fw_version=2019.01-V01.00.00.2-0-g8e86139. I have corrected the boot order after installing the /etc/fw_env.config file. But I still cannot get the example image V1.1.1 to finish posting. I can get the same boot sequences result as these two threads: problems-booting-image-v1-1-1 iot2050-bricked It looks like a known problem. One resolved it using Example Image V1.0.2. So I have started trying to build V1.0.2 following this guide how-to-build-github-example-image, but 4 tasks are failing. /repo/recipes-app/npm/npm_6.10.3+ds.bb:do_fetch Thanks. |
Follow us on