(0)| 6/2/2009 12:01 PM | |
|
Joined: 1/4/2007 Last visit: 12/16/2025 Posts: 1197 Rating:
|
Hello dBigD, It is not really clear for me, how much is the dead load of the mechanics in your case. It is necessary, that the dead load plus the load must be less than the nominal load (=rated load into the attached catalogue). You can use for example one SIWAREX WL260 SP-S SA load cell (see the page 3/16 of the attached catalogue), if the platform has the max. size of 400 x 400 mm. On that platform, you can mount the conyevor. If you are using a 20 kg SIWAREX WL260 SP-S SA load cell, you will reach an accuracy of 11 g. If you are using a 50 kg SIWAREX WL260 SP-S SA load cell, you will reach an accuracy of 27 g. In any case, I recommend you to use a stainless steel load cell (e.g. SIWAREX WL260 SP-S SA), because a stainless steel load cell has less vibrations than an aluminium load cell. Best regards Siwarexi AttachmentWT10_2009_03_Load_Cells.pdf (487 Downloads) |
Follow us on