(0)| 8/21/2023 7:33 AM | |
|
Joined: 4/20/2023 Last visit: 12/4/2024 Posts: 33 Rating:
|
I have a simovert masterdrive 6SE7087 working in a system with S7 300. Now I want to control it with new controlling system (including S7 1200 and ET200SP) using analog and digital IN/Out . I connected the the terminals (X101 and X102) as it was defined in the working system. For digital IN/Out it's working fine but analog IN/Out it's not working fine, I can't get the right value for tourqe and actual speed. For analog input of ET200SP I'm using "AI 8xI 2-/4-wire BA". I set both channel to 4-20mA and tried both 2wire and 4wire transducer but could not read the right value. Defined parameter of the Masterdrive and also wiring of the masterdrive to S7 300 can be find in the attachements. AttachmentSimovert.zip (685 Downloads) |
Follow us on