8/21/2023 7:05 AM | |
Joined: 6/26/2023 Last visit: 9/2/2025 Posts: 25 Rating:
|
Hi everyone, Attachmentpng2pdf.pdf (520 Downloads) |
8/21/2023 8:09 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, as the S7-1500 should be used as slave, you need the GSD for the S7-1500 and configure this in the project of Yokogawa. How to you connect the communication module CM 1542-5 or the communications processor CP 1542-5 as I slave in STEP 7 V5.x to an S7-300/S7-400 CPU?-> also works with another Master PROFIBUS GSD files: SIMATIC-> use GSD file according your ET200SP CPU + CM DP regards sancruz |
Last edited by: sancruz at: 08/21/2023 08:11:17Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on