8/21/2023 1:37 PM | |
Joined: 8/21/2023 Last visit: 4/16/2025 Posts: 1 Rating:
|
Hi, I need your help about a problem. The readout of HSC input with 1 S7-1215C has troubles. As you can see in this short video, the HSC input readout increase with a big step at the end without reason, there is no disturbance on the input. I have 5 flowmeter connected to this PLC and only the first one has problem. Do you know where I did a mistake ? Is the problem can be link to use the %I0.0 for the flowmeter and I used the MB0 clock in the program ? Thanks in advance Attachmenttest.avi (455 Downloads) |
Follow us on