(0)| 9/12/2023 8:41 AM | |
|
Posts: 1 Rating:
|
I am trying to get tags from S7 200 Smart PLC (ST60) to SCADA, using SIDIRECT OI driver, to show the data on Intouch SCADA. However, I'm stuck at figuring out the correct TSAP setting for the S7 200 Smart. I tried different combinations as in s7-200 smart 如何设置TSAP | 找知识-找PLC (zhaoplc.com), but none of them really worked (I put in remote tsap of the SIDIRECT configuration). My station has 3 modules, the PLC + 2 EMs. I also tried to read the tag via S7 PC Access Smart but without success (tried different TSAP as well) So I am not sure if I miss anything, or I can find the TSAP parameter of the PLC anywhere on the Microwin S7 Smart software ? I'm new to S7 200 Smart so really need help. AttachmentS7_200_Smart.zip (649 Downloads) |
| 9/12/2023 8:58 AM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello, it's hard with SMART family here to give some clear support. I recommend this Topic about some little knowledge or find FAQ about TSAP description. I don't know if you say that you did some combinations with tests, it is like run on mine field... Update: here is also another document about TSAP wit ISO on TCP protocol but can give also some knowledge to you: TSAP configuration with ISO on TCP protocol |
Last edited by: Duris_I at: 09/12/2023 09:52:08With best regards... |
|
Follow us on