(0)| 9/14/2023 12:13 AM | |
|
Joined: 4/28/2015 Last visit: 8/25/2025 Posts: 4 Rating:
|
After enable PUT/GET in s7-1500 PLC, WinCC OA can communicate with s7-1500 PLC by s7 protocol driver; while WinCC 7.5 cannot communicate with it by s7 protocol suite. Anyone can give me some hints about the difference between these two protocol driver? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/14/2023 10:24:05New subject after splitting |
|
| 9/15/2023 11:38 AM | |
|
Joined: 5/30/2022 Last visit: 12/17/2025 Posts: 634 Rating:
|
Hi AutoGen_951566, I am not aware of the WinCC OA part but in WinCC V7.5 for communication between an S7-1200 and an S7-1500 a specific driver "Simatic S7-1200 S7-1500 Channel" is used and not the protocol suite which is for the 300 and 400: "SIMATIC S7-1200, S7-1500 Channel" channel This 1200-1500 driver works through the TCP/IP protocol and allows you to bring the symbols directly from the PCL, for example |
|
If this information really helps, you could use the Rate function. |
|
Follow us on