10/3/2023 2:09 AM | |
Joined: 12/8/2022 Last visit: 1/23/2024 Posts: 1 Rating:
|
I see this is a very old post but I'm hoping to revive it. I am wanting a function that you can input a running time of a piece of equipment and the running average would be calculated to a maximum of X hrs. to help operators see when the process started to trend in a bad direction. I have seen it in a Emerson Delta V and I think I have also seen it in an ABB Freelance and XA system. Just hoping someone can point me in a direction. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/09/2023 04:36:26New subject after splitting |
|
10/5/2023 5:30 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, I have not checked these blocks in detail, but maybe you can build something own out of these: Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500-> LGF_FloatingAverage (FB / V3.0.2) -> LGF_AverageAndDeviation (FC / V3.0.1) regards sancruz |
Feedback appreciated, please rate |
|
Follow us on