9/29/2023 5:57 AM | |
Joined: 3/28/2015 Last visit: 8/15/2025 Posts: 725 Rating:
|
Hello,, 1-Did you do the setting in the HMI? Control Panel-------> Transfer------->.......... 2- Check PG/PC settings |
Eng.Mohamed Ibrahim |
|
9/29/2023 3:24 PM | |
Posts: 2 Rating:
|
Hello Mohamed, yes, transfer mode is active. In the PG/PC interface settings we have PC/PPI cable active |
10/5/2023 1:33 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16349 Rating:
|
Hello InstandhaltungBitzer Check this FAQ: https://support.industry.siemens.com/cs/de/de/view/28928853 then if you have a Field PG then there is a Profibus/MPI CP integrated. you would also be able to do the backup/Restore by DP/MPI. If you have donw already a OS Update by Prosafe then there is no Project loaded on the panel any more. you would have to load the project from WinCC flexible again. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on