(0)| 10/6/2023 12:37 PM | |
|
Posts: 2 Rating:
|
Hello! I was trying to get this script up and running so that I can acknowledge alarms from the external button connected to the PLC, however I think I`m missing some details. The way I tried to do the ACK is that I put an IO field "under" the alarm viewer with the PLC Acknowledge signal connected to process value field. Afterwards, I`ve added script to the "Change" parameter for the Process value, but it doesn`t work. Could anyone help on this matter ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/09/2023 10:26:58New subject after splitting |
|
Follow us on