10/10/2023 7:28 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi Roby, Have you changed the resolution? Because from what I see, the text adjustment issue has been corrected but now the resolution is not set correctly. Make sure that both the resolution and the text setting are the same (in the IPC and in the HMI). Or if you increase the resolution, does the other problem come back? Try playing with these values to adjust it to the screen. Best regards.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on