1/9/2023 11:27 AM | |
Joined: 6/1/2020 Last visit: 8/21/2024 Posts: 41 Rating:
|
I am reading some examples about clients created in C# using some libraries from Siemens. Some cases use Opc.UA.Core.dll and Opc.UA.Client.dll, like in this example (June 2022): Creating of OPC UA clients with .NET and helper class - ID: 109737901 - Industry Support Siemens In another cases are used the opcrcw.comn.dll and the opcrcw.da.dll. Like in this example (September 2022): SYH_OPC_76.pdf - SIMATIC NET: PC software Industrial Communication with PG/PC Volu... - ID: 77376110 - Industry Support Siemens So I am wondering which is the difference between them and which could be more suitable in my case. Are there more libraries? There is some way where I could find this kind of resorces instead using the find tool and take them from the code of the example? |
Last edited by: Jen_Moderator at: 01/09/2023 12:53:52Links optimized. |
|
4/17/2023 9:03 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16349 Rating:
|
Hello GTSAGarcia To give another example for the collection https://support.industry.siemens.com/cs/de/en/view/109748892 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on