(2)| 10/27/2023 3:44 PM | |
|
Joined: 12/18/2014 Last visit: 1/11/2026 Posts: 36433 Rating:
|
I'm sorry, but what is a "SZVTNMV018092"? |
| 10/27/2023 6:21 PM | |
|
Posts: 7 Rating:
|
My mistake. That's the number on the side next to the barcode so I thought that was the model number. Model number is 6ED1 052-1MD00-0BA5 |
| 10/28/2023 4:02 PM | |
|
Joined: 6/11/2019 Last visit: 1/9/2026 Posts: 2720 Rating:
|
Hello DMirabella, Yes, something like that is possible with the Logo 5. A program often says more than a thousand words.So here's an example in the appendix: B014 = filling time for small cup B015 = Filling time for large cup B001 = Changeover time to manual filling B009 = Blocking time so that the operator can select the large cup without the time for the small cup starting. Of course you have to adapt the times to the system and your wishes. Greetings Ella_68 (translated with Google) Attachmentautomat_0ba5.zip (637 Downloads) |
| 11/1/2023 9:28 AM | |
|
Joined: 6/11/2019 Last visit: 1/9/2026 Posts: 2720 Rating:
|
Hello DMirabella, Your old LOGO!Soft should run on its own. At least you can upgrade it to the current version for free. You can find the link here in the forum. I have attached the program as a PDF. Greetings Ella_68 (translated with Google) AttachmentLOGO!Soft Comfort - automat_0ba5.pdf (946 Downloads) |
Follow us on