(0)| 12/8/2023 9:41 PM | |
|
Joined: 2/10/2021 Last visit: 9/7/2025 Posts: 2 Rating:
|
Can anyone explain the behavior in the image attached here? Specifically, - the counter B008 can only increment if the value of Q2 is 0 and the value of Q3 is 1 - Q3 feeds the Q2 Relay Coil, so the Q3 Relay Coil should be evaluated before the Q2 Relay Logic - If the value of Q3 is 1, then, because that Q3=1 feeds an OR instruction before the Q2 Relay Coil, the logic feeding the Q2 Relay coil should never write a value of 0 to Q2 when Q3 is 1. The environment is LOGO!Soft Comfort Demo version 8.3.0 (2021-03-08 13-30) running the Simulator. More detail on the application is available at this link. |
Last edited by: drbitboy at: 12/08/2023 21:41:51 |
|
| 12/9/2023 3:20 AM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36380 Rating:
|
Please upload the program as a ZIP file. Your link leads to a website that requires you to log in. |
Follow us on